XX – Input, Counter view parameters (5034-UB8, 5034-UB8F)

The
XX – Input, Counter
view includes these parameters:
Parameter
Description
Power Source
Defines the power source for the point.
  • Ptxx – Power is supplied to the sensor from point xx of this module, which is configured to function as a power supply.
    If a short circuit is detected on the Power Supply point, the fault is rolled-up to the Digital Input point.
  • External – Power is supplied to the sensor from an external power supply.
  • SSV – Power is supplied to the sensor from the SSV terminal of this module.
    If an SSV short circuit is detected, the fault is rolled-up to the Digital Input point.
Input Filters
Off → On Filter Time
Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid.
Input Filters
On → Off Filter Time
Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid.
Preset
Displays the value, set in the output tag Preset, to use for counter preset. The value can range from 0…2,147,483,647.
Rollover at Preset
Determines the action that is taken when the input tag Count reaches the output tag Preset value.
  • If selected, the counter counts to the Preset value, rolls over to zero, and then sets the Rollover bit. The Done bit is not set.
  • If cleared, the counter counts to the Preset value and sets the Done bit, then continues counting up to the maximum DINT value. The Rollover is set when Count transitions from 2,147,483,647 to 0.
Counter State in Program Mode
(For 5034-UB8F only)
Determines the behavior of each counter when the controller transitions to Program Mode or Inhibit mode. While in Program Mode or Inhibit mode, the counter behaves as follows:
  • Countinue counting
  • Hold – Retain the last count and resume counting from this count when the controller transitions to Run Mode.
  • User-defined value – Set the count to the user-defined value and resume counting from this value when the controller transitions to Run Mode.
Counter State in Program Mode
User-defined Value
(For 5034-UB8F only)
Defines the value that is set to count when Counter State in Program Mode is selected as User-defined value.
Counter State in Communication Fault Mode
(For 5034-UB8F only)
Determines what happens to the counter after a communication fault occurs and the module enters Communication Fault Mode.
  • Countinue counting
  • Hold – Retain the last count and resume counting from this count when the controller transitions to Run Mode.
  • User-defined value – Set the count to the user-defined value and resume counting from this value when the controller transitions to Run Mode.
Counter State in Communication Fault Mode
User-defined Value
(For 5034-UB8F only)
Defines the value that is set to count when Counter State in Communication Fault Mode is selected as User-defined value.
Counter State When Communication Fails in Program Mode
(For 5034-UB8F only)
Determines the counter action if communication fails in Program Mode.
  • Program Mode – Follow the behavior for Program Mode.
  • Communication Fault Mode – Follow the behavior for Communication Fault Mode.
Diagnostics
Opens the Diagnostics dialog, which contains diagnostic information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal