Commission a Safety System

Figure 1 shows the steps that are required to commission a safety system when you use
FactoryTalk® Design Studio
to create your project.
An independent, third-party safety assessment can be required before the system is approved for operation. An independent, third-party certification can be required for IEC 61508 SIL 2 or SIL 3 levels.
Commission a Safety System
Commission a Safety System
Complete the following steps to create a safety system with
FactoryTalk® Design Studio
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal