Validate the Project
To check your application program for adherence to the specification, you must generate a
suitable set of test cases that cover the application. Document and retain the set of test
cases as the test specification. To determine what to validate for your specific application,
refer to IEC 61508 or your industry-specific safety standard.
You must include a set of tests to prove the validity of your application logic. These tests
are within the defined value ranges, at the limits, or in invalid value ranges. The necessary
number of test cases depends on safety application.
Active validation with field devices must also be included, as it is the only way to verify that the sensors and actuators in the system are wired correctly. Verify the operation of programmed functions by manipulating sensors and actuators manually.
You must also include tests to verify the reaction to wiring faults and network communication faults.
Project validation includes tests of fault routines, and input and output channels, to be sure that the safety system operates properly.
To perform a project validation test on the controller, you must perform a full test of your
application. You must activate each sensor and actuator that is involved in every safety
function. Be sure to test all shutdown functions, because these functions are not exercised
during normal operation.
Also, know that a project validation test is valid only for the specific application tested. If the safety application is moved to another installation, you must perform startup and project validation on the safety application in the context of the new sensors, actuators, wiring, networks, and control system physical equipment.
Revalidation Considerations
The IEC 61508 functional safety standard requires an impact analysis before you upgrade or
modify components in a certified, functional safety system. Reference the standard to make
sure that you fulfill all requirements as they relate to your application. Consider the
following high-level information for impact analysis of safety controller software,
hardware, and firmware modification.
- All major and minor firmware releases for safety controller systems are certified for use in safety applications. As part of the certification process,Rockwell Automation®tests the safety-related firmware functions, such as the safety communication subsystems, which are embedded safety instruction execution, and safety-related diagnostic functions. The firmware release notes identify changes to safety-related functions.
- Perform an impact analysis of the planned modifications.
- Review the firmware andFactoryTalk® Design Studio™release notes for changes in safety-related functionality.
- Review the hardware and firmware compatibility in the Product Compatibility and Download Center (PCDC) to identify potential compatibility conflicts.
- Plan, analyze, and document the impact of any modification, enhancement, or adaptation of your validated safety system.
- As part of the upgrade process, remove and regenerate the safety signature.
- Based on the results of the safety impact analysis, choose the appropriate level of hardware and software revalidation.
- If you already have a signed safety application that is validated with an earlier version ofFactoryTalk® Design Studio™and the safety signature matches after you deploy using a newer version ofFactoryTalk® Design Studio™, no revalidation is necessary.
- If you have conducted testing of an unsigned safety application with an earlier version ofFactoryTalk® Design Studio™, you must rerun those tests with the new version ofFactoryTalk® Design Studio™.TIP: We recommend that you generate a safety signature before testing your safety application.
Provide Feedback