Safety System Principles

You must read, understand, and fulfill safety requirements as described in this publication before you operate a SIL 2/PLd or SIL 3/PLe safety system.
FactoryTalk® Design Studio
is certified to clause 7.4.4 of IEC 61508-3 Edition 2 only when used according to this publication.
You, the user, own, specify, design, develop, test, and validate any safety system that you create with
FactoryTalk® Design Studio
.
You must be trained and experienced in safety applications before you develop the application program for the intended SIL 2 or SIL 3 system. You must follow good design practices.
  • Use functional specifications, including flowcharts, timing diagrams, and sequence charts.
  • Perform a review of safety task logic.
  • Perform application validation. As you develop your safety application, consider the following important notes.
IMPORTANT:
  • FactoryTalk® Design Studio
    is certified to clause 7.4.4 of IEC 61508-3 Edition 2 and can be used during the coding lifecycle of applications and also as an aide in the module test, integration test, and validation test lifecycle phases. As a result, no additional justification for its use during those lifecycle phases is required. If, however, other tools are used, either on their own or with
    FactoryTalk® Design Studio
    , additional justification for those other tools is required. It is your responsibility to verify that other offline tools that are used during all lifecycle phases are selected as a coherent part of the software development activities.
  • You are responsible to conduct an assessment to determine the level of reliance that is placed on
    FactoryTalk® Design Studio
    and the potential failure mechanisms that can affect the executable software when the application is used in a manner other than what is specified in the product documentation.
  • You must verify that all programming and configuration information that is entered into
    FactoryTalk® Design Studio
    , and deployed to the controller, meets the requirements for your application.
  • When connecting to a safety controller, the application compares the serial number of the controller with the last known serial number an application was deployed to. A warning displays, which you must acknowledge, if the application detects a mismatch. To avoid faults, verify the serial number with the product label on the safety controller. Any other means of verification requires confirmation of the accuracy of the serial number.
  • As required by the safety integrity level, the software, or design representation, the characteristics of the application must be compatible with the features
    FactoryTalk® Design Studio
    supports and the safety controllers that are listed in the Preface.
  • As required by the safety integrity level, the software or design representation must be compatible with the features that are supported in
    FactoryTalk® Design Studio
    and safety controllers. It is your responsibility to verify that the desired software and design representation are supported in
    FactoryTalk® Design Studio
    and safety controllers. For example, if the design is represented in a flowchart format, it is your responsibility to convert that design to a ladder diagram.
  • The use of third-party, internally developed, or artificial intelligence tools to generate logic automatically to import into
    FactoryTalk® Design Studio
    for compilation and deployment to a controller requires assessment of the tool's suitability at the point in the development cycle where it is selected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal