Safety Concept
The safety concept assumes the following requirements.
- You are responsible to create, operate, and maintain the safety application.
- You are fully qualified, specially trained, and experienced in safety systems.
- You apply the logic correctly to detect programming errors through strict adherence to specifications, programming, and naming rules.
- You must confirm that the Ladder Diagram logic is entered correctly inFactoryTalk® Design Studio™. Use the Code Editor and Commit History comparison tools to review the textual representation of the logic code. We strongly recommend that multiple people review the code.
- You must confirm that the safety-related parameters (safety-related properties of safety objects and safety tag values) are correct in the safety controller before you generate a safety signature. These values can change after application deployment. Use the Safety Confirmation Report to review the parameters (see Confirm the Project).
- You perform a critical analysis of the application and use all possible measures to detect a failure.
- You confirm all application deployments with a manual check of the safety signature.
- You perform a complete functional test of the entire system before the operational startup of a safety-related system. This test includes, but is not limited to, the following.
- Validate that the overall functionality of the implemented safety functions, including I/O configuration via Add-on Profiles, beyond the limits of the individual devices (boundary testing).
- Verify that the correct versions of software are used.
Status | Safety Rating (Up to and Including) | Controller Behavior |
|---|---|---|
No signature | Only for development purposes |
|
Unlocked with signature | SIL 3/PLe/Cat. 4 control reliable |
|
Locked with signature | SIL 3/PLe/Cat. 4 control reliable |
|
IMPORTANT:
To achieve the safety ratings listed in Table 1, you must adhere to the safety requirements defined in this
safety reference documentation.
Provide Feedback