Lock the Controller

See Safety Application Lock/Unlock for information about the safety lock feature. When you deploy to a locked safety controller,
FactoryTalk® Design Studio
performs an internal check to see if safety changes occurred in the offline project since the last deployment. You can only deploy if no safety changes are present. Otherwise, you must safety-unlock the safety controller before deployment.
  1. See Deploy a project to a controller in the FactoryTalk Design Studio Online Help for instructions on how to use
    FactoryTalk® Remote Access
    Manager to deploy an application.
IMPORTANT: If you change the safety controller application after the initial safety-lock, you must first safety-unlock the safety controller to deploy, which deletes the safety signature. You must manually regenerate a new safety signature after deployment.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal