Secure Web Server
The PointMax EtherNet/IP adapter allows you to view network diagnostic information and
configure network settings of the module through a secure web server interface.
To view the web server interface, enter the IP address of the adapter into your browser,
preceded by “https://”.
For example, https://192.168.1.99
IMPORTANT:
Make sure that your LAN and TCP/IP settings are configured to access the subnet
on which your adapter communicates.
We recommend that you only use a secure network environment as it retains default
settings.
Provide Feedback