Reset the Adapter

To reset the PointMax EtherNet/IP adapter to its default settings, complete the following steps.
  1. Power down the adapter.
  2. Set the rotary switches to 888.
  3. Power up the adapter.
  4. Wait for the adapter power-up sequence to complete.
    The power-up sequence is complete, and the adapter has returned to its factory default setting when the status indicator states are as follows:
    • Ok indicator is flashing red.
    • All other indicators are off.
  5. Power down the adapter.
  6. Set the rotary switches to the desired address.
    IMPORTANT:
    If you do not want to set the IP address via the rotary switches, set them to 999.
    After the adapter powers up, set the IP address.
  7. Power up the adapter.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal