모션 오류
다음 다이어그램은 Logix Designer 응용 프로그램과 관련된 축 오류(축 및 모션 그룹 오류)를 계층 구조로 표시합니다. 이러한 오류가 적용되는 축(Axis) 유형의 약어가 각 오류 옆 괄호 안에 표시됩니다.
기호 | 축(Axis) 유형 |
C | AXIS_CONSUMED |
CD | AXIS_CIP_DRIVE |
S | AXIS_SERVO |
SD | AXIS_SERVO_DRIVE |
V | AXIS_VIRTUAL |
![]() | ![]() | |
![]() | ||
![]() | ![]() | ![]() |
![]() | ![]() | |
AuxFeedbackFault (SD) CommutationFault (SD) DriveCoolingFault (SD) DriveFault (S) DriveHardFault (SD) DriveOvertempFault (SD) FeedbackFault (S,SD) GroundShortFault (SD) MotFeedbackFault (SD) MotorOverloadFault (SD) MotorOvertempFault (SD) NegSoftOvertravelFault (S, SD) OverSpeedFault (SD) PositionErrorFault (S,SD) PosSoftOvertravelFault (S, SD) PowerPhaseLossFault (SD) CIPAxisFaults (CD) MotorOvercurrentFault MotorCommutationFault MotorOverspeedFLFault MotorOverspeedULFault MotorOvertemperatureFLFault MotorOvertemperatureULFault MotorThermalOverloadFLFault MotorThermalOverloadULFault MotorPhaseLossFault InverterOvercurrentFault InverterOvertemperatureFLFault InverterOvertemperatureULFault InverterThermalOverloadFLFault InverterThermalOverloadULFault ConverterOvercurrentFault ConverterGroundCurrentFLFault ConverterGroundCurrentULFault ConverterOvertemperatureFLFault ConverterOvertemperatureULFault ConverterThermalOverloadFLFault ConverterThermalOverloadULFault ConverterACPowerLossFault ConverterACSinglePhaseLossFault ConverterACPhaseShortFault ConverterPreChargeFault BusRegulatorOvertemperatureFLFault BusRegulatorOvertemperatureULFault BusRegulatorThermalOverloadFLFault BusRegulatorThermalOverloadULFault BusRegulatorFault BusModuleFault BusUndervoltageFLFault BusUndervoltageULFault BusOvervoltageFLFault BusOvervoltageULFault BusPowerLossFault BusPowerBlownFuseFault BusPowerLeakageFault BusPowerSharingFault FeedbackSignalNoiseFLFault FeedbackSignalNoiseULFault FeedbackSignalLossFLFault FeedbackSignalLossULFault FeedbackDataLossFLFault FeedbackDataLossULFault FeedbackDeviceFault SensorFault BrakeSlipFault HardwareOvertravelPositiveFault HardwareOvertravelNegativeFault ExcessivePositionErrorFault ExcessiveVelocityErrorFault OvertorqueLimitFault UndertorqueLimitFault ExcessiveBusVoltageErrorFault AmbientTemperatureRiseFault IllegalControlModeFault EnableInputDeactivatedFault ControllerInitiatedFault ExternalInputFault CIPAxisFaults2 (CD) ACLineOvervoltageFLFault ACLineOvervoltageULFault ACLineUndervoltageFLFault ACLineUndervoltageULFault ACLineHighFrequencyFLFault ACLineHighFrequencyULFault ACLineLowFrequencyFLFault ACLineLowFrequencyULFault ACLineVoltageUnbalanceFault ACLineCurrentUnbalanceFault ACLineVoltageSagFault ACLineFrequencyChangeFault ACLineSyncLossFault ACLineSyncFailureFault InverterGroundCurrentFLFault InverterGroundCurrentULFault InverterOutputPhaseShortFault AuxiliaryPowerSupplyFLFault AuxiliaryPowerSupplyULFault BusInputOvercurrentFLFault BusInputOvercurrentULFault CIPAxisFaultsRA (CD) CommutationStartupFault MotorVoltageMismatchFault FeedbackFilterNoiseFault FeedbackBatteryLossFault FeedbackBatteryLowFault FeedbackIncrementalCountErrorFault ControlModuleOvertemperatureFLFault ControlModuleOvertemperatureULFault ConverterPreChargeOverloadFLFault ConverterPreChargeOverloadULFault ExcessiveCurrentFeedbackOffsetFault RegenerativePowerSupplyFault PWMFrequencyReducedFault CurrentLimitReducedFault TorqueProveFault DecelOverrideFault PreventativeMaintenanceFault MotorTestFault HardwareConfigurationFault FirmwareChangeFault ConverterPreChargeInputDeactivatedFault DCCommonBusFault RuntimeErrorFault BackplaneCommunicationErrorFault SafetyModuleCommunicationErrorFault ACLineContactorFault ACLineResonanceFLFault ACLineResonanceULFault TrackStopFault LostMoverAssociationFault UnassociatedMoverFault PeripheralHardwareFLFault PeripheralHardwareULFault PeripheralOverTemperatureFLFault PeripheralOverTemperatureULFault PeripheralUnderTemperatureFLFault PeripheralUnderTemperatureULFault PeripheralCommunicationFLFault PeripheralCommunicationULFault AdapterCommunicationFLFault AdapterCommunicationULFault MechanicalBrakeOutputFault ExcessiveMotorVoltageFeedbackOffsetFault ACLinePhaseReversalFault PhaseThermalImbalanceFault DCBusVoltageImbalanceFault PredictiveMaintenanceFault ProductSpecificFault | ControlSyncFault (SD, CD) ModuleHardwareFault (S,SD, CD) ModuleSyncFault (S,SD, CD) TimerEventFault (S,SD, CD) SERCOSRingFault (S,SD) ModuleConnFault (CD) ConnFormatFault (CD) LocalModeFault (CD) CPUWatchdogFault (CD) ClockJitterFault (CD) CyclicReadFault (CD) CyclicWriteFault (CD) ClockSkewFault (CD) ControlConnFault (CD) ClockSyncFault (CD) LogicWatchdogFault (CD) DuplicateAddressFault (CD) SystemConnectionFault (CD) | |
의견을 작성 부탁드립니다.