Process tab
The following are the settings on the tab of the
Process
FactoryTalk Resource and Status
Server Properties
dialog. It shows when Enable data from workstation and processed monitoring
is selected.Setting | Description |
|---|---|
Add | Opens the Add Process dialog to add processes that you want to monitor. |
Delete | Deletes the processes that you select. |
Export | Exports the process list as a CSV file. |
Import | Imports a CSV file that contains the process list. |
Process Name | Shows the name of the processes that you want to monitor. |
Alias Name | Enters the alias name processes. It is optional. |
Fournir une réponse