General tab

The following are the settings on the
General
tab on the
FactoryTalk Resource and Status
Server Properties
dialog.
Setting
Description
Name
Enters the FactoryTalk Resource and Status server name. The name cannot be changed after the server is created and cannot include dashes or hyphens.
Description
Enters the description for the FactoryTalk Resource and Status server.
Interval between update cycles (seconds)
Configures the time interval between each data update cycle.
FactoryTalk Resource and Status server computer
Enters the computer name that hosts the FactoryTalk Resource and Status server If you want to change the FactoryTalk Resource and Status server computer, enter another computer name, or
Browse
for another computer.
Enable data from FactoryTalk Diagnostic Counter Monitor
Enables the FactoryTalk Resource and Status server to get data from FactoryTalk Diagnostic Counter Monitor.
Enable data from workstation and processes monitoring
Enables the FactoryTalk Resource and Status server to monitor the data from workstations and processes.
Enable Ethernet device status detection
Enables the FactoryTalk Resource and Status server to monitor the connection data from Ethernet devices.
Fournir une réponse
Vous avez des questions ou des commentaires sur cette documentation ? Veuillez envoyer vos commentaires ici.
Normal