Device Status tab
Frequent updates for a high number of addresses may cause network congestion. The following are the settings on the tab.
Device Status
Setting | Description |
|---|---|
Number of addresses to ping as a group | Configures the device quantity in a group to ping simultaneously. |
Interval between each ping group (seconds) | Sets the time interval between each ping group. |
Interval between each complete cycle group (seconds) | Sets the time interval between each data collection cycle of all devices. |
New | Adds one or multiple device addresses manually. |
Delete | Deletes one or multiple device addresses. |
Export | Exports the device address list as a CSV file. |
Import | Imports a CSV file that contains the device address list. |
Fournir une réponse