Add a device address
Add one or multiple device addresses that you want to monitor.
To add a device address
- On theDevice Statustab, selectNew.
- Enter a device address that you want to monitor, such as IPv4, hostname, or DNS.The alias name is optional.
- SelectApplyto save the changes.
Fournir une réponse