Data from workstations
The following are the data from workstations. This information can normally be found by accessing the Windows operating system Task Manager’s
Performance
tab.Component | Parameter | Description | Type | Unit |
|---|---|---|---|---|
CPU | Processes | Shows the number of processes using the server host's CPU. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Numeric | N/A |
SpeedMHz | Shows the CPU speed. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Numeric | Megahertz | |
UtilizationPercent | Shows the CPU usage percent. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Numeric | Percent | |
Disk | TotalGB | Shows the total space of all computer's hard disks. This attribute is retrieved from Windows and can be viewed in the Windows File Explorer . | Numeric | Gigabyte |
TotalGB.C | Shows the total space of drive C. C means the drive name. If the multiple drives in a computer are monitored, all drives will be listed. This attribute is retrieved from Windows and can be viewed in the Windows File Explorer . | Numeric | Gigabyte | |
UsedGB | Shows the used space of all computer's hard disks. This attribute is retrieved from Windows and can be viewed in the Windows File Explorer . | Numeric | Gigabyte | |
UesedGB.C | Shows the used space of drive C. C means the drive name. If the usage for multiple drives in a computer is monitored, all drives will be listed. This attribute is retrieved from Windows and can be viewed in the Windows File Explorer . | Numeric | Gigabyte | |
Memory | AvailableGB | Shows the amount of memory which is available for allocation to a new process or to existing processes. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Numeric | Gigabyte |
CommitedGB | Shows the physical memory in use for which space has been reserved in the paging file should it need to be written to disk. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Numeric | Gigabyte | |
InuseGB | Shows the amount of memory being used by applications. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Numeric | Gigabyte | |
TotalGB | Shows the total memory space. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Numeric | Gigabyte | |
Network | AdapterName | Shows the network adapter name. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Text | N/A |
IPv4 | Shows the IPv4 address. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Text | N/A | |
IPv6 | Shows the IPv6 address. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Text | N/A | |
ReceiveKbps | Shows the average number of bytes per second received by the process in the last minute. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Numeric | Kilobyte per second | |
SendKbps | Shows the average number of bytes per second sent by the process in the last minute. This attribute is retrieved from Windows and can be viewed on the Task Manager’s Performance tab. | Numeric | Kilobyte per second |
Fournir une réponse