Add a process
Add one or multiple processes running on the computer hosing the FactoryTalk Resource and Status server to monitor.
To add a process
- On theProcesstab, selectAdd.
- In theAdd Processdialog, select a method to add a process.
- Add from Task ManagerIt is only available for the local host.Select one or multiple processes, and then selectOK. Use theRefreshfunction to get the latest data and theSearchfunction to find the desired process.
- Add by process nameSelectNew, enter the process name that you want to monitor, and then selectOK.
- SelectApplyto save the changes.
Fournir une réponse