Add a graphic element to a project
Create screen content by adding graphic elements from the
Toolbox
or drawing free-form shapes. Rockwell Automation
recommends using no more than 500 graphic elements, including image graphic elements, on a screen.After adding a graphic element to a screen, control its appearance and behavior by changing its properties, binding it to a tag, and associating it with an animation or event.
Provide Feedback