Lock or unlock graphic elements
Lock graphic elements to prevent them from moving when developing a screen or the definition of an Add-On Graphic. Locked graphic elements cannot be selected or affected by keyboard or mouse input. Locking a graphic element does not affect the application on the HMI device. Locking screens and popups is not supported.
To lock or unlock a graphic element:
- In theGraphic Explorer, point to the graphic element.
- Tolocka graphic element, selectUnlock
. Unlockchanges toLock
to indicate the graphic element is locked. - Tounlocka graphic element, selectLock
. Lockchanges toUnlock
to indicate the graphic element is unlocked.
Provide Feedback