Download and run a Machine Edition Runtime (MER) application

Download and run a Machine Edition Runtime (MER) application to update a
PanelView Plus
with the latest
FactoryTalk ViewPoint for Machine Edition
displays.
Prerequisites
To download and run an MER application
  1. In
    FactoryTalk View Studio
    , from the
    Tools
    menu, select
    Transfer Utility
    .
  2. In the
    Source file
    area, click the
    Browse
    button (...), select a MER file, and then click
    Open
    .
  3. In the
    Select destination terminal
    list, browse for and select a
    PanelView Plus
    .
  4. Click
    Download
    .
  5. When the download completes, click
    OK
    , and then click
    Exit
    .
  6. On the
    PanelView Plus
    operator terminal, open the
    FactoryTalk View ME
    Station
    configuration screen.
  7. Click
    Load Application
    , select the MER file that was downloaded, and then click
    Load
    .
  8. Click
    Run Application
    to start the application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal