Create a Machine Edition Runtime (MER) application
Create a Machine Edition Runtime (MER) application to include
FactoryTalk ViewPoint
displays on the operator terminal. If any changes have been made to the displays since the last time they were published, FactoryTalk View Studio
automatically re-publishes the displays and includes them in the .mer (MER) file when it is created.
IMPORTANT:
Language switching is not supported in
FactoryTalk ViewPoint
. The web content is published in the default language of the FactoryTalk View
application. To change the default language, use the Tools > Languages
menu in FactoryTalk View Studio
.Prerequisites
To create a runtime application
- In, from theFactoryTalk View StudioApplicationmenu, selectCreate Runtime Application.
- In theCreate Runtime Applicationdialog box, select the MER settings:
- File name- Enter the name for the MER file.
- Save as type- Select a runtime version that is compatible with the firmware of the operator terminal.
- Conversion to development application- Select whether the MER file can be used to generate a .med (MED) file.
- EnsureInclude ViewPoint contentis selected.
- (optional) Select theFactoryTalk ViewPoint versionfrom the list.
- ClickSave.
- In theCreate Runtime Application Wizard - Select Languagesdialog box, select which languages will be included in the application and which language will be the initial language.
- ClickFinish.
Provide Feedback