Publish graphic displays
Publish graphic displays to convert selected
FactoryTalk View
displays into FactoryTalk ViewPoint
displays.Prerequisites
- Select aFactoryTalk Viewapplication.
- Select graphic displays.
To publish graphic displays
- On thePublish Displays to Webscreen, clickPublish displays.The status column updates as each display is published. The progress bar displays overall publication progress.TIP:
- To cancel publishing, clickCancel.
- To resume canceled publishing, or to select different screens to publish, clickSelect displays.
Provide Feedback