Select graphic displays
Select graphic displays to publish them to
FactoryTalk ViewPoint
. Displays that have changed since the last publication are automatically selected for publication.If you are publishing displays for the first time, or if the selected
FactoryTalk View
application does not match the currently published application, then initially all displays are automatically selected for publication.The
Initial Display
selection can be superseded by a macro with an associated Display
command.
IMPORTANT:
Language switching is not supported in
FactoryTalk ViewPoint
. The web content is published in the default language of the FactoryTalk View
application. To change the default language, use the Tools > Languages
menu in FactoryTalk View Studio
.Prerequisites
- Select aFactoryTalk Viewapplication.
To select graphic displays
- On thePublish Displays to Webscreen, clickSelect displays.FactoryTalk ViewPoint Administrationlists all the displays in the selected application. If you do not see the displays, expand the application's area or HMI server in the list.
- In theWeb Enablecolumn, select whether each display should be published:
- Selected - The display will be published.
- Cleared - The display will not be published.
- In theInitial Displaycolumn, select which display will be shown when a user connects toFactoryTalk ViewPoint.
- (optional) SelectRe-publish all selected displaysto overwrite the existing published displays even if their content has not changed.
Provide Feedback