Configure the FactoryTalk ViewPoint server
The
FactoryTalk ViewPoint
server is included as part of the .mer file that runs on the PanelView Plus
graphic terminal. It hosts the published web application and provides client licenses to web browsers that connect to the application. Use FactoryTalk ViewPoint Administration
to configure session expirations for a FactoryTalk ViewPoint
terminal.Provide Feedback