Change the FactoryTalk ViewPoint for Machine Edition inactivity timeout
Change the inactivity timeout to adjust how often a user must change displays or refresh a page. If the inactivity timeout is reached, the web browser's session expires.
Prerequisites
- Ensure the operator terminal is running theFactoryTalk ViewPoint for Machine Editionapplication.
To change the
FactoryTalk ViewPoint for Machine Edition
inactivity timeout- Open a web browser toFactoryTalk ViewPoint Administrationat the following URL, replacingcomputer_name_or_ip_addresswith the hostname or IP address of thePanelView Plusoperator terminal:http://computer_name_or_ip_address/ftvp/adminIf the site has an HTTPS binding, enterhttpsinstead ofhttp.
- (optional) If web application security is enabled, enter your username and password, and then clickOK.
- On theServer Settingstab, select theEnablecheckbox and then inInactivity Timeout, type a value for the number of minutes that a session can be inactive.A value of 0 disables the inactivity timeout. The default value is 20 minutes.
- ClickApplyto save your changes.
Provide Feedback