About activation and licenses

FactoryTalk ViewPoint
embeds a single license in the
PanelView Plus
firmware that allows a single client connection.
A
FactoryTalk ViewPoint
license is not required to open
FactoryTalk ViewPoint Administration
, but only one connection can be made at a time.
Normal Operation
When a client web browser connects to a published web application, the
FactoryTalk ViewPoint
server loans its license to the web browser. The license allows the web browser to view the application in up to three browser windows or tabs. If a second browser attempts to connect to the
FactoryTalk ViewPoint
server, the "No licenses available" error message is shown.
The license is released immediately upon signing out from the web application, or within 30 seconds of disconnecting a web browser from the server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal