Trends
A trend is a visual representation or chart of the current or
historical tag values. A trend provides an operator with a way to track plant activity
as it is happening.
In FactoryTalk View SE, you can create two different types of trending objects:
- The TrendPro objects provide modern trending capabilities witheasy runtime configuration, drag and drop ad-hoc trending, and statistical and sampling calculations.
- The Trend objects provide traditional trend functionality.
Provide Feedback