Set trace properties as default (TrendPro)
Trace properties and Y-axis properties
can be saved as default in the test run mode or at runtime on the current computer. The traces you create afterwards will inherit the default properties you configured earlier.
To set trace properties as default
- After you have configured the trace and Y-axis propertiesin the test run mode or at runtime, right-click a trace on the canvas or a trace (or a row) in theTrace Listtable, and then selectSet Trace as Default.
Provide Feedback