RecipePro+

A recipe is a specific set of numeric and string data values (ingredients) that are associated with a specific set of tags. The function of recipes is to allow a runtime operator to write each data value to its associated tag in one operation.
Each ingredient has a pre-set data value assigned to it. The set of numeric and string tags assigned to the ingredients in the recipe is called a tag set. The ingredients, tag sets, and data values are stored together in a recipe file, all arranged in an easy-to-use spreadsheet.
Each ingredient must have a unique name. A recipe can have up to 15,000 ingredients. You can edit, import, or export recipes at design time and runtime. You can also write the recipe data values to tags, or write tag values to recipes at runtime.
The recipes can be used for manufacturing food and beverages. They can also be used for any application where you want to show, edit, or save multiple values at once. For example, recipes are used in the petrochemical and pharmaceutical industries. In the pharmaceutical industry, you could use recipes to design flexible packaging, creating recipes that specify the number of tissues to put in a box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal