About the RecipePro+ editor
How do I open the RecipePro+ Editor
In
FactoryTalk View Studio
, in the Explorer window, under the HMI server, double-click RecipePro+
> RecipePro+ Editor
.The RecipePro+ editor extends the functionality of the Recipe editor with advanced recipe management. You can use the RecipePro+ editor to create, duplicate, edit and preview the recipes. By refreshing recipe values, you can view the differences between the current tag values and the preset recipe values. You can also use it to export recipes to CSV files or import recipes from CSV files.
By using the
FactoryTalk View
command RecipeProEdit
, you can open the RecipePro+ editor with full functionality at runtime. In this case, you do not need a FactoryTalk View Studio
license. You can also open the RecipePro+ editor with fewer functionalities by using the FactoryTalk View
command RecipeProList
.
TIP:
The earlier operations are initiated by RecipePro+ commands that are assigned to the actions of graphic objects. Therefore, there must be a graphic object like a button on the display for each operation that you want to perform. For details about using the
Command Wizard
and about specific FactoryTalk View
commands, see FactoryTalk View SE
Help.The RecipePro+ editor consists of these parts:
- ToolbarContains commonly used actions, such as creating, deleting, and refreshing recipes. When you point to an icon on the toolbar, its description is displayed below it.
- Navigation barContains tabs to edit, import, or export recipes. You can click the left-pointing or right-pointing pointer at the bottom to collapse or expand the tabs.
- Recipe file editorProvides an editable area where you can set up and configure recipes, specify importing or exporting options.TIP:TheCurrent HMI Serverlist is not available at design time. It is only available at runtime.
Provide Feedback