Save recipe values
At runtime when you double-click the recipe object, the Recipe dialog box is displayed. You can use it to save recipe information to disk or restore values from the selected file to the input objects in a graphic display.
To save recipe values from a graphic display to a recipe file:
- At runtime, in a graphic display, double-click therecipeobject.
- In the Recipe dialog box, type the name of the file in theRecipe Filefield or click the down arrow to display the list of existing recipes and choose one of them.
- ClickSaveto transfer the values from the input objects in the graphic display, to the selected recipe file.
You can also use the
RecipeSave
command to save values to a recipe file.Provide Feedback