Restore recipe values
At runtime when you double-click the recipe object, the
Recipe
dialog box is displayed. You can use it to save recipe information to disk or restore values from the selected file to the input objects in a graphic display.To restore recipe values in a graphic display from the recipe file:
- At runtime, in a graphic display, double-click therecipeobject.
- In theRecipedialog box, type the name of the file in theRecipe Filefield or click the down arrow to display the list of existing recipes and choose one of them.
- ClickRestoreto transfer the values from the selected recipe to the input objects in the graphic display.
You can also use the
RecipeRestore
command to restore values from a recipe file.After restoring values from a recipe file to input objects in a display, to download the values, press
PgDn
, or use the DownLoad
or DownLoadAll
command.Provide Feedback