About input objects at runtime

You can use input objects at runtime to send data to a tag in a tag database or network device, or to retrieve and display data from one. You can change retrieved data in the input objects, then download the new values to tag. Input objects are also used with recipes to download values from a group of input objects. Enter information in numeric input objects in the numeric format specified by the
Regional Settings
in the Windows
Control Panel
.
You can also use some keys or commands with input objects at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal