Import recipes
Use the RecipePro+ editor to import recipes from CSV files.
The imported recipe names are the same as the CSV file names. For example, if the CSV file is
Sugar.csv
, the recipe name after importing is Sugar
.To import recipes:
- In the RecipePro+ editor, on the navigation bar, selectImport.
- In theCurrent HMI Serverlist, if needed, select another HMI server where you want to import.TIP:The list is not available at design time. It is only available at runtime.
- Select an import option:
- To skip existing recipes with the same names and only import the new recipes, selectImport new recipes and add to existing recipes.
- To replace existing recipes with the same names and import the new recipes, selectImport new recipes and replace existing recipes.
- ClickImport from.
- In theOpendialog box, select one or more CSV files you want to import and clickOpen.
- When complete, to view the log of the import process, clickView log file.
Provide Feedback