Export recipes
Use the RecipePro+ editor to export recipes to CSV files for massive edits with spreadsheet programs like Microsoft Excel.
Each recipe will be saved to a CSV file with the same name as the recipe. For example, the recipe
Sugar
is saved to Sugar.csv
.To export recipes:
- In the RecipePro+ editor, on the navigation bar, selectExport.
- In theCurrent HMI Serverlist, if needed, select another HMI server where the recipes are.TIP:The list is not available at design time. It is only available at runtime.
- Beside theExport tofield, clickBrowseto select a folder where you want to export and clickOK.
- UnderRecipes selection, select the recipes you want to export.
- ClickExport.TIP:If you have files with the same names in the specified folder, the exported files will replace the existing files.
- When complete, to view the log of the export process, clickView log file.
Provide Feedback