Start FactoryTalk View ME Station automatically on a PanelView Plus CE terminal from Windows Startup folder
On a
PanelView Plus CE
terminal, you can start FactoryTalk View ME Station
automatically whenever the terminal starts by setting up the startup options or follow the steps below.To start
FactoryTalk View ME Station
automatically when a PanelView Plus CE
terminal starts- Copy the path to the MERuntime.exe file (FactoryTalk View ME Station) to the WindowsStartupfolder.The default folders of the path to the MERuntime.exe file is\Storage Card\Windows\Desktop.The WindowsStartupfolder is\Storage Card\Windows\Startup.TIP:If you copied the path to the MERuntime.exe file to the WindowsStartupfolder, to disable the automatic startup ofFactoryTalk View ME Station, delete the file in the Windows Startup folder.
Provide Feedback