Save the edited Unicode text file in Excel

When you complete editing an exported Unicode text file in Excel, save the file in Excel.
To save the edited Unicode text file in Excel
  1. In Excel, from the
    File
    menu, select
    Save As
    .
  2. Make sure that
    Unicode Text (*.txt)
    is selected in the
    Save as type
    box and click
    Save
    .
  3. When the message appears stating that the file may contain features that are not compatible with Unicode Text and asking if you want to keep the workbook in this format, click
    Yes
    . This saves the file but does not close it.
  4. Close the file in Excel. When asked whether you want to save the changes, click
    Save
    . You can then save the file using its original name or specify a new name.
  5. When prompted with the same message described in Step 3, click
    Yes
    .
    TIP:
    • If a Unicode text file has been opened and saved in Excel, and you open the file in Notepad, the double quotes surrounding the string definitions will have been removed for most strings.
    • String definitions containing embedded double quotes or other characters that Excel treats as special characters (such as commas) will be enclosed within double quotes. Any embedded double quotes will have been converted to a pair of double quotes. The
      FactoryTalk View
      String Import Export Wizard imports all of these correctly.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal