Edit an exported Unicode text file in Notepad

You can edit an exported Unicode text file in Notepad.
To edit an exported Unicode Text File in Notepad
  1. Open the file in Notepad. The first seven lines of the file explain what cannot be edited. The text strings that can be edited are enclosed in double quotes.
  2. Make the changes required to translate the strings.
  3. From the
    File
    menu, select
    Save As
    . Make sure that
    Text Documents [*.txt]
    is selected in the
    Save as type
    box, and
    Unicode
    is selected in the
    Encoding
    box. Save the file using its original name or specify a new name.
  4. Close the file and Notepad.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal