Edit an exported Unicode text file in Excel
You can edit an exported Unicode text file in Microsoft Excel (recommended).
To edit an exported Unicode text file in Excel
- Open Excel, and from theFilemenu, selectOpen.
- In theOpendialog box, make sure thatAll Filesis selected, select the file you are going to edit, and clickOpen. The Text Import Wizard opens.
- In Step 1 of the Text Import Wizard, select the following options and clickNext:
- Choose the file type that best describes your data: Delimited
- Start import at row: 1
- File origin: Windows (ANSI)
- In Step 2, select the following options and clickNext:
- Delimiters the data must contain: Tab(make sure the other check boxes are cleared.)
- Treat consecutive delimiters as one: clear the check box
- In Step 3, forColumn data format, selectGeneral.
- ClickFinish.
The first seven lines of the Unicode file explain what you can and cannot change in the file.
Provide Feedback