Import text strings from a Unicode text file

You can import text strings from a Unicode text file into an application.
Prerequisites
  • Make sure that the application that you are going to import text into is not being edited or modified.
  • Create a backup of the text currently in your application by exporting it. This allows you to restore the original text to the application if an error occurs while importing, or if you cancel the import before it is complete.
To import text strings from a Unicode text file
  1. In the
    Language Configuration
    dialog box, select the language to import and click
    Import
    .
  2. In the
    Import Operation
    dialog box, select
    Import strings from a Unicode file into<
    RFC1766
    >
    .
  3. Select a file to import text strings from.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal