Transfer a file from a MobileView, PanelView Plus 7, PanelView Plus 6, PanelView Plus, PanelView Plus Compact, or PanelView Plus CE terminal
Use the
Upload
tab of the Transfer Utility
dialog box to transfer runtime application files (.mer) from a MobileView
, PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, or PanelView Plus CE
terminal to a development computer.Before you transfer an application file, you must configure an
FactoryTalk Linx
driver for the transfer on the terminal and the computer.To transfer a file from a
MobileView
, PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, or PanelView Plus CE
terminal- On theUploadtab of theTransfer Utilitydialog box, from theSelect source terminallist, select the source terminal in theFactoryTalk Linxcommunications tree.
- From theSource storage typelist, select the kind of storage the file is stored in on the terminal.
- In theSource filebox, specify the file to be transferred. Click theBrowsebutton to browse for the file.
- (Optional) If you want to use a different name for the uploaded file, selectUpload asand type the new name.
- In theDestination folderbox, specify the location on the destination computer to upload the file to. Click theBrowsebutton to browse for the destination.TIP:The destination must be on the local computer. ME Transfer Utility does not support uploading to a network location.
- ClickUpload.
The selected file starts to be uploaded to the destination folder.
Provide Feedback