Options on the Upload tab
The following table shows the options on the
Upload
tab.Options | Descriptions |
|---|---|
Source storage type | Options include:
|
Source file | Type the path to the source file or click the Browse button (…) to open the Select File dialog box, browse for the source file, and click OK . |
Upload as |
|
Destination folder | Specify where on the destination computer you want to store the file. |
Select source terminal | The FactoryTalk Linx communication tree shows all the hardware available on the network. |
Provide Feedback