Methods

A
method
is an action or subprogram that an event performs under certain circumstances.
An event performs a method when:
  • An event occurs at runtime
  • An event required by a runtime C# script occurs at runtime
  • A request from an OPC UA client occurs at runtime
  • A C# script runs at design time
You can associate multiple methods with a single event. When the event occurs, the methods are performed in the order in which they were added to the event at design time. A method can have properties or input or output arguments. Use input arguments to specify values that the method displays when the event occurs, such as incrementing the value of a graphic object. Output arguments are values that the method returns. As with variables, the value of an argument can be fixed or dynamic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal