Create a method for an object
Create a method for an object to be performed at runtime. Create a method for a runtime
NetLogics that you add to
Project view
.- InProject view, select the object node.
- Selectand then select
Runtime NetLogic.Runtime NetLogic#appears inProject view. - Right-clickRuntimeNetLogicand select .NetLogicopens in the editor with added code:[ExportMethod] public void MethodName() { // insert code to be executed by method }
- (Optional) Rename the method in C#.
runtime netlogics
Runtime Netlogics
Provide Feedback