Delete a method from an event

Delete an event to remove the event and the event methods from the project. You cannot delete the default events for a pre-configured element.
  1. In
    Project view
    , select an object.
  2. In
    Properties
    under
    Events
    , expand the user-defined event.
  3. Select the event and then press
    Delete
    .
The event is removed from the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal