Add Enterprise

Enterprise is the highest in the hierarchy list and each tenant has a single Enterprise.
NOTE:
The following points are required to view data on
Enterprise level dashboard
:
  • For Cost charts, the respective rate schedule must be configured at the Site level.
  • For Emission, the respective emission factor must be configured at the Site level.
  • For Production, energy intensity charts must have correct tag mapping for production count measurement.
  • For more than one resource meter harmonized unit defined at the Enterprise level can be used for displaying data for consumption, intensity & emission.
Perform the following steps to create an Enterprise:
  1. On the left navigation menu, click the
    Settings
    drop-down and click
    Configuration
    .
    Add Node
  2. Click
    Add Node
    .
    The
    Add Node
    dialog box is displayed.
    Add Enterprise Dialog
  3. In the
    Add Node
    dialog box, set these parameters:
    • Name
      : Provide an Enterprise name.
    • Currency
      : Select a currency from the drop-down list.
    • Description
      : Provide a description of the Enterprise.
    NOTE:
    The user can configure currency at the Enterprise level.
  4. Click
    Add
    .
The "
Enterprise added to hierarchy successfully
" message is displayed.
Related Information
:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal