Edit Enterprise Default Unit
Perform the following steps to configure the Default unit at the Enterprise level:
- Click theDefault unittab.
- On the required default unit, click the [
] icon.
- TheEdit Unit Configurationdialog box is displayed. Edit the required fields.
- ClickSave.Enterprise Default UnitThe "Unit configuration changes updated successfully" message is displayed.
Provide Feedback