Function block diagram elements

Function block diagram (FBD) elements are the components that build an FBD program. All the elements listed in the following table can be added to an FBD program in
FactoryTalk Design Workbench
.
FBD program elements
Element
Description
Elements that store and process information.
Instructions including operators, functions, and function blocks (including user-defined function blocks).
Connection point for the input variable that the function block uses to perform its operations.
Connection point for the output variable that the function block uses to perform its operations.
Connection point for the input or output variable that the function block uses to perform its operations.
Free-format text that can be inserted anywhere in the FBD program.
Descriptions are for documentation purposes only and are not acted upon by the program.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal