Add an instruction block

When creating a function block diagram (FBD) program, an instruction block is used in the FBD language editor.
A functional element in an FBD program can be an instruction block, a function, a user-defined function block, or an operator.
FBD instruction block example
FBD instruction block example
To add an instruction block
  1. In
    Toolbox
    , in
    Search
    , enter the instruction block name.
  2. Drag the instruction block to the editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal