Add a variable, input reference, or output reference

Variables, input references, and output references are connection points that the function block uses to perform its operations.
  • Variables are connections points for input and output variables.
  • Input references are connection points for input variables.
  • Output references are connection points for output variables.
To add a variable, input reference, or output reference to an FBD program
  1. From
    Toolbox
    , drag one of the following to a valid location:
    • Add variable button for a variable.
    • Input reference button for an input reference.
    • Output reference button for an output reference.
  2. Assign a variable by doing one of the following:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal