Add a description

Descriptions are free-format text that can be inserted anywhere in the function block diagram (FBD) program. Descriptions are for documentation purposes only and are not acted upon by the program.
To add a description
  1. From
    Toolbox
    , drag Add description button to the editor.
  2. In the text box, enter the description.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal