Communication diagnostics

The communication diagnostics pages show the real-time statistics of the controller's Ethernet, DeviceNet, or serial port connections.
When the
Micro800
controller is connected, the pages show statistics depending on the controller's communication configuration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal